9/2/2018 1:14 PM | |
Posts: 12 Rating:
|
thank you for your quick answer. i am using tia portal v12 i already used it to create a HMI, i was wondering is there any other graphic display beside the one i putted in the attachement section ? Does the ktp 1000 PN allow me to put a usb flash disk to do data acquisition from the HMI in the cvs fromat ? ------------------------------------------------------------------------------------------ |
Last edited by: Kach_man at: 9/2/2018 1:17:45 PMLast edited by: Jen_Moderator at: 9/5/2018 12:33:59 PMNew subject after splitting |
|
9/2/2018 2:26 PM | |
Joined: 12/18/2014 Last visit: 11/29/2023 Posts: 31497 Rating:
|
Unfortunately, I have no TIA V12, only V13, V14 and V15. That's why I can not create an example. As far as I know, V12 did not have a special communication driver for LOGO !, so you had to select the S7-200 driver (not S7-1200). On this Siemens website Application examples for LOGO! is there an example of communication between LOGO! and Siemens HMI. HMI communication starting from WinCC V11.x (TIA Portal)
I can not answer that question, it does not belong in the LOGO! conference, but in the HMI conference. |
Follow us on