9/23/2016 2:58 PM | |
Posts: 24 Rating: (0) |
Hi to all, where can I find other graphics to WinCC Basic?. Especially bar graphs and process indicators. Thank you
|
9/23/2016 3:36 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (192) |
Hello Ferdinando, if you click on the "Libraries" button on the right side of the screen you'll find a library named "Monitoring-and-control-objects. You might not be able to use all of them on your Basic Panel. Here are two bar controls that work:
You can't use the "normal" gauge-control on a Basic Panel, but here is a version you can use:
What controls do you think of if you say "process indicators"? Under "Toolbox > Graphics > WinCC Graphics Folder > Unified and modular" you can find several graphics which you can use in a graphics list to indicate different statuses of objects/proecesses. For example signal towers ('traffic light') or a motor/fan/pump/... in different colors to show the status of the device. |
Last edited by: H.J. at: 9/23/2016 3:37:42 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to3 thankful Users |