3/14/2018 9:39 AM | |
Joined: 1/6/2009 Last visit: 1/28/2025 Posts: 136 Rating:
|
Hello everybody, I'm trying to download a project with COMTEXT to an OP15. The program was uploaded from another OP15 and when I try to download it to another one, in the middle of the process the COMTEXT simply shutdown and I need to chose "terminate drivers" to open it again. During the upload it uploads the system fine and during the objects upload it happens. I already try to upload another programs (smaller programs) and the upload is done successfully. Do someone know what can cause this problems? Regards, Nuno |
3/14/2018 1:37 PM | |
Joined: 4/28/2015 Last visit: 2/24/2025 Posts: 10832 Rating:
|
Hello, I had lot of problems with OP15 in my history, also HW malfunctions - memory corruption,... Maybe also this can be similar problem of memory problem. Do you have chance to make some memory test in init of boot? What I remember some diagnostic was performed after boot and prior download??? Check in manual. |
With best regards... |
|