12/21/2007 1:15 PM | |
Joined: 4/24/2006 Last visit: 3/19/2025 Posts: 8903 Rating:
|
Hello _instrument, Have you seen this faq: http://support.automation.siemens.com/WW/view/en/10420976 Did you in properties of PC-adapter (setting PG/PC interface) select 'PG is only master on the bus'? Best regards, Wizard |
12/1/2017 7:01 PM | |
Joined: 6/1/2013 Last visit: 11/8/2024 Posts: 10 Rating:
|
I'm also facing with this problem "Communication link to the adapter damaged". I have reinstalled the simatic manager but still no solution. In the PG/PC interface "PG/PC is the only master on the bus" is selected. MPI adapter details:6ES7972-OCB20-0XA0. Communication with the TCP/IP is ok. Please suggest what I can do to resolve the communication issue with the MPI adapter. Thanks In Advance Regards Satish Pandey
|
Follow us on