1/11/2024 8:46 PM | |
Joined: 11/24/2018 Last visit: 8/28/2024 Posts: 29 Rating: (1) |
Hello Experts! A happy New Year to all. I have uploaded the parameter file from a Micromaster 440 via a USB-to-Serial adaptor attached to my PG M5, Windows 7 Ultimate. That worked fine, but the download to a new (identical) Micromaster 440 failed. See picture attached! I can seen on the PG as well as on the front display of the inverter, that some parameters have made it through the download, even though, ultimately, it ended with an error. Needless to say, that the drive also does not work as before or at all. The "Help" file points into the direction of "Write protection - p7760". I cannot find this parameter, even in the "Expert list". I've run out of things to try; hence this post. Any help would be very welcome. Thank you very much and have a great day! Thx. DBME ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/12/2024 09:56:03New subject after splitting |
|
Follow us on