1/16/2020 6:25 PM | |
Joined: 12/19/2012 Last visit: 5/6/2024 Posts: 3 Rating: (0) |
Hi all, i have to download the SPW420 software to an empty T400, the card code 6DD1606xxxx and the CD rom is 6DD1843-OAA0 we have the 3pins cable and all software (i think), Step7 5.4, CFC and D7-Sys, but i really don't know how to transfer the package, other than setting dip switch S1-7 to ON. The drive is a MDVV CUVC 3.3, and the original DriveMonitor file backup tells the t400 has d000=420 and d001=2.2 What do I need to open and how to transfer via the serial link using DUST1? Thank you in advance, final user is pushing me a lot. Pier ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 01/16/2020 18:30:37New subject after splitting |
|