12/19/2016 5:21 PM | |
Joined: 1/6/2009 Last visit: 1/28/2025 Posts: 136 Rating:
|
Hi, I tried to transfer a wincc program to a mobile panel 177b trought profibus but I can't detect what I'm doing wrong. I follow this instructions https://support.industry.siemens.com/cs/document/23802404/how-can-you-transfer-a-wincc-flexible-project-via-mpi-profibus-to-a-windows-based-panel-?dti=0&lc=en-WW When I try to detect the panel with profibus test in step7 everything apears except the panel. I set up the transfer settings in the panel, with exactly the same settings of the the old panel that was in the machine, address, speed, etc, and I can detect the old panel but when I put the new one I have nothing there in the net. The only thing wich is missing to test is to use the new panel with the cable of the old one. Because we test it with a cable we have here but it can be a used one. But despite of this test we will do tomorrow can you se something tha can be missing in the configuration? Thank you all. |
Follow us on