8/5/2016 5:10 PM | |
Posts: 35 Rating: (0) |
I too am having problems downloading to a KTP700 Basic DP. I have an S7-200 which I am having to program with Microwin and the KTP700 which I have written the program with TIA Portal V13 sp1. The software is completely up to date, but when I come to download, it only gives me the option for Teleservice, nothing else. This is the first time I have used Portal so you will have to excuse my shortcomings. I have checked the means of download in the project tree and that says ok. Any help would be very appreciated. Rob ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 8/7/2016 10:38:02 AMNew subject after splitting |
|
8/8/2016 9:55 AM | |
Posts: 35 Rating: (0) |
Hi again, Can I just email you the project? I think I am missing something, settings or missing info. Regards Rob |
8/8/2016 11:17 AM | |
Posts: 35 Rating: (0) |
OK Christoph, I have done as you said. The image is attached. Regards, Rob |
8/8/2016 11:45 AM | |
Posts: 35 Rating: (0) |
Can I communicate with USB if a USB selection is made. Is the USB lead a standard A - B USB lead. Regards, Rob |
8/8/2016 11:55 AM | |
Posts: 35 Rating: (0) |
Christoph, What do I need to do to put the situation right. Regards, Rob |
8/8/2016 11:56 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
Hello, the Basicpanel have no USB port for a connection to PC.
Christoph |
8/8/2016 1:15 PM | |
Posts: 35 Rating: (0) |
Christoph, The system for the TIA is windows 7 ultimate x86. Regards, Rob |
8/8/2016 1:50 PM | |
Posts: 35 Rating: (0) |
Christoph, I think I have found the section you are referring to, but what are the subkeys? Regards, Rob |
8/8/2016 1:55 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
Hello, provide a screen of you registry tree then i can answer this question exactly
Christoph |
8/8/2016 2:06 PM | |
Posts: 35 Rating: (0) |
Christoph, I don't usuall go into the settings, that's why I don't know this. Regards, Rob |
8/8/2016 2:29 PM | |
Posts: 35 Rating: (0) |
Hi Christoph, I deleted all the keys that you said, but unfortunately it is the same as before. Regards, Rob |
8/8/2016 2:32 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
Hi, can you check if the registry key's was created again after the TIA Start? Christoph |
8/8/2016 2:39 PM | |
Posts: 35 Rating: (0) |
Hi, No they haven't. Rob |
8/8/2016 3:06 PM | |
Posts: 35 Rating: (0) |
Hi Christoph, Surprisingly it worked!! I will check it in portal now to see if it is there. Rob |
8/8/2016 3:56 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
Hello, a USB Port 3.0 is blue colored , this adapter was not released for USB 3.0. Christoph |
8/8/2016 4:08 PM | |
Posts: 35 Rating: (0) |
Hi, Definitely USB2 then, I haven't got any blue ports. Rob |
8/8/2016 4:12 PM | |
Posts: 35 Rating: (0) |
Hi Christoph, I have another laptop, I could try to put TIA Portal on that, see what happens. Regards, Rob |
8/10/2016 5:09 PM | |
Posts: 35 Rating: (0) |
The second screenshot. |
8/10/2016 7:55 PM | |
Posts: 35 Rating: (0) |
All sorted Christoph, Many thanks for your help, you pointed me in the right direction. Regards, Rob |
Follow us on