3/20/2025 10:39 AM | |
Joined: 7/10/2024 Last visit: 4/24/2025 Posts: 169 Rating:
|
Hello! In the following link you can find the corresponding image. - Image Downloads for SIMATIC HMI Operator Panels: Comfort / Mobile / Basic Panels Besides, I suggest you always use the latest version available, which in this case would be the V17 update 8 for comfort panels. This way you make sure that you are working on the most developed version. Anyway, I attach the following FAQ that I think will be quite useful for you. - Error when loading the project into an HMI Panel with Firmware adaption |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
Follow us on