Industry Online Support
Technical Forum
6/25/2009 9:29 AM | |
Posts: 262 Rating: (45) |
Dear Firend, Please understand system diagnosis can only be carried out when AS-interface is integrated in an automation system with a joint database. DP/ AS-i link advance has user friendly display for Fault list for AS-i Line etc. You can use AS-I Analyzer; an external diagonstic & test Unit, it gives you complete diagnosis for for system.( like it could be internal EEPROm error, periphery fault, if it is configuration mode etc). Please refer the attched doument for the same. Moroever, it is recommended to download system Manaul of this site. MLFB of System Manual is 3RK27033BB021AA1. AttachmentDiagnosis of AS-i Router.zip (129 Downloads) |
Follow us on