1/31/2016 10:40 AM | |
Joined: 5/1/2013 Last visit: 1/22/2025 Posts: 428 Rating:
|
Hello I have a problem with dp communication. As shown in "attached pdf file I have consisted system, " CPU-317 2pndp, drives, and 3 pieces of Touch panel. PLC program STEP7 V5.5 SP4, HMI has made a WINCC V13 SP1.
When I plug in CP5711 other place like OP1, there is no problem with dp communication. Some suspect the reason, but I do not know the exact reason. 2: The connection between the DP connector is not good. (Some DP connector already tried to connect again.) AttachmentQ.pdf (45 Downloads) |
Follow us on