2/16/2010 6:35 PM | |
Joined: 1/4/2008 Last visit: 1/4/2025 Posts: 703 Rating: (96) |
Hello, the reason is that the DP/DP coupler is writing this bit to tell you the comm is OK and data are transfered succesfully, it could be setby DIA switch on coupler (if I remember well, it's switched on by default). Look to the manual for the DP/DP coupler, chapter 4.2.2. Regards Sydney |
Last edited by: Sydney at: 2/16/2010 6:45 PM |
|
This contribution was helpful to1 thankful Users |
2/16/2010 7:18 PM | |
Posts: 8946 Rating: (999) |
That is correct. Also, in the manual you will find the recommention, NOT to use the first byte for inputs if you are using the DIA - Bit! |
This contribution was helpful to1 thankful Users |
Follow us on