6/18/2014 9:30 PM | |
Posts: 8946 Rating:
|
Looks fine... Do you monitor the status using variable statusscreen? Do you test all Bytes, not only the first? What are the adresses of the slots(I/Q)? |
6/19/2014 11:34 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello Ktsui, In addition to our friend IBN-Service have a look perhaps might help you: Behavior of the DP/DP coupler when a master system fails or look our Expert Fritz: DP Coupler no data exchange. |
Last edited by: Ste39 at: 6/19/2014 11:43 AMLast edited by: Ste39 at: 6/19/2014 11:42 AM |
|
This contribution was helpful to
2 thankful Users |
6/20/2014 6:17 AM | |
Posts: 4 Rating:
|
Dear IBN-Service, >>What CPU? 6ES7 412-3HJ14-0AB0 and 6ES7 151-8FB01-0AB0 >>RED LED on CPU? Yes, but since I have created a new program for testing the coupler, I haven't config others connected modules in HW configuration. >>Prozess Image is large enough? Process image inputs: 2048 bits Process image Outputs: 2048 bits Is that not large enough? >>You see on BOTH sides just the DIAG-Bit, nothing else? Yes. >>You are shure that you set the outouts in sending PLC? Yes. I have attached the testing program. (I changed the IO slots address from 200 to 0) Regards, Ktsui Dear ste39, Thanks for your help Regards, Ktsui AttachmentTest_DP_.zip (100 Downloads) |
6/20/2014 9:35 AM | |
Joined: 10/7/2005 Last visit: 7/25/2024 Posts: 3011 Rating:
|
Hello Ktsui your Process Image is certainly large enough, problem is that none of your DP/DP coupler I/O modules are using it. By default the should be assigned to "OB1 PI", but in your case none of them is assigned to "OB1 PI" nor any of the PIP's (Process Image partitions). Anyhow, the fix is simple, double click on each I/O moduleof your DP/DP coupler and select "OB1 PI" from the drop down list as per attached pic. I hope this helps |
Cheers |
|
This contribution was helpful to
3 thankful Users |
6/20/2014 9:20 PM | |
Posts: 8946 Rating:
|
|
This contribution was helpful to
2 thankful Users |
6/21/2014 7:00 AM | |
Posts: 4 Rating:
|
Thank you very much, everyone. Problem solved. Regards, Ktsui
|
This contribution was helpful to
3 thankful Users |
Follow us on