Industry Online Support
Technical Forum
2/1/2009 5:10 AM | |
Joined: 9/27/2006 Last visit: 9/24/2023 Posts: 12153 Rating:
|
Hello; Have you had a look at the function FB126 "PNIODiag". I worked with its predecessor, FB125, and it was an excellent provider of information on failed Profibus-DP nodes. Screens for WinCC and WinCC Flexible were attached so you could display at least the functionnal status of each node. FB126 is an enhanced version 0f FB125, with the capability to include Profinet IO nodes in diagnostic mode. Have a look at the Application note on FB126, determine if it will respond to your requirements. http://support.automation.siemens.com/WW/view/en/26996747 Hope this helps, Daniel Chartier |
2/5/2009 10:24 AM | |
Joined: 10/3/2008 Last visit: 9/20/2023 Posts: 946 Rating:
|
Hi, have a look at this: Systemdiagnostics. This addon is easy to implement in an existing project as well and a very powerful addon. Wüstenräuber |
Follow us on