2/19/2021 8:49 AM | |
Joined: 9/26/2019 Last visit: 9/8/2022 Posts: 3 Rating:
|
Thank you for the info. I'll use the ZSW1 from the PLC tags to get the alarm bit. |
2/19/2021 11:15 AM | |
Joined: 10/11/2006 Last visit: 1/27/2023 Posts: 5404 Rating:
|
as mentioned the TO provides the status. Additionally there is the possibility to read or write parameters of the S210 via the library LacycCom (acyclic communication). You can also use the message handling available on Siemens Support , so that error messages of the drive are displayed in plain text.https://support.industry.siemens.com/cs/ww/en/view/109479553 |
With best regards, |
|
Follow us on