9/10/2022 1:55 PM | |
Joined: 9/21/2012 Last visit: 2/19/2025 Posts: 4280 Rating:
|
There has to be some entrys in the alarm buffer, check it out. |
This contribution was helpful to
1 thankful Users |
9/17/2022 3:42 AM | |
Joined: 5/9/2011 Last visit: 10/16/2024 Posts: 71 Rating:
|
I have tried to re-commission the drive numerous times unfortunately no success. What I can see now when looking into the PLC program is that the drive stops when "frequency reached"bit is activated. When looking at the frequency feedback from the drive it seems that the setpoint is written directly into the feedback word the moment you start the drive. Currently I am using telegram 1 with NIST_A as the frequency feedback. This is connected to r63(0) "Actual speed unsmoothed". I am also attaching the STARTER project. AttachmentGcb12ap.zip (348 Downloads) |
Follow us on