9/9/2015 2:07 PM | |
Joined: 5/12/2006 Last visit: 3/20/2025 Posts: 22572 Rating:
|
Hello, do you find the PLC if you start accessible Nodes or edit ethernet nodes? Regards Christoph |
9/10/2015 10:57 AM | |
Posts: 160 Rating:
|
Hi, I'd say that no further drivers are required. In the pg/pc interface you need to select your Ethernet chip, one that is integrated into your PC/Laptop. As you already said, you have to set IP's of your PLC and PC where only the last set of numbers have to deffer (X.X.X.1 and X.X.X.10 for example). If you have already change IP address of PLC, sometimes it is useful to perform memory reset. Then go to the Accessible Devices and your PC should automatically recognize your PLC, as you may see in photo. Janko Attachmentphoto (2).DOCX (227 Downloads) |
9/11/2015 7:53 AM | |
Joined: 5/12/2006 Last visit: 3/20/2025 Posts: 22572 Rating:
|
Hi, is the laptop connected to the PLC or to the CP343 ? Rregards |
Follow us on