7/22/2020 8:35 AM | |
Joined: 11/14/2018 Last visit: 4/3/2025 Posts: 502 Rating:
|
Hello mcandeo, this discussion might help you: Beside that, it's important that you give information about the WinCC you're using. (Basic/Comfort/Advanced/Professional). When you ask a question, you can basically always have a look at the following post, it explains which information are needed: Regards, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
This contribution was helpful to
1 thankful Users |
8/13/2020 2:21 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello If you have a Comfort/Advanced Project: https://support.industry.siemens.com/cs/de/en/view/57025748 If you have a WinCC Professional RT Project then you can use a Combobox Object and load the Values with a VB Script like this (Script Context is for example in the same Screen in Event Screen Loaded): Dim ComboObj and so on, its just a small example to guide you i the right direction. And next Time a few more Information would be very nice... Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on