Industry Online Support
Technical Forum
7/19/2006 2:06 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
If you don't mind a simple "left to right" fill then you can do the following : Draw a Smart Object -> Bar on the screen Set the Axis and Line Weight property to 0 Draw a polygon over the top of the bar to shape it into your required shape Set the polygon background colour to the picture colour and set the Line Width to 0 This will then give the effect of a shape filling. I have attached my example, done in V6 SP4. Another way would be to draw the object twice, with two different colours,and have a script that resizes the second object to create a fill effect. You could do this with a polygon but it would involve some pretty tricky scripting. Attachmentfilling.zip (96 Downloads) |
Follow us on