9/25/2024 6:26 AM | |
Joined: 3/25/2015 Last visit: 10/2/2024 Posts: 49 Rating: (9) |
Hello everyone, To start off and so I don´t forget, I am using TIA Portal V19 Upd. 2 and the current project is a unified comfort panel MTP1200 I have a question/problem concerning dynamic SVGs. I have been playing around with dynamic SVGs and creating my own to integrate into future projects and added them into "Program Files\Siemens\Automation\Portal V19\Data\Hmi\SvgControls". All was going great until I archived the project and passed it along to a college. All the dynamic SVGs were missing for him when he opened the project. After some searching I found out I was doing it wrong and the correct way is to create a folder in the project itself under <project_folder>/UserFiles/SVGControls (Link). The problem I am having is that this folder is not appearing in the Dynamic widgets drop down list. I have all the requirements for it to work but it doesn't. Requirement
When I open the demo project from Siemens "Feature demo + TechShowCase demo". They have some custom dynamic SVGs in the demo located in <project_folder>/UserFiles/SVGControls and it shows up in the dynamic widgets list as Project Graphics So the big question is what am I doing wrong for it not to work on my project? Has anyone encountered this problem? or any ideas what I could be doing wrong? Thanks |
Last edited by: Moderator_Lan at: 09/25/2024 07:15:45links optimized |
|
Follow us on