Industry Online Support
Technical Forum
5/1/2012 7:21 AM | |
Posts: 13 Rating: (0) |
please answer this question for me as in need to know the answer urgently .pls help |
5/1/2012 10:59 AM | |
Posts: 57 Rating: (0) |
Dear Piku, The isolation monitor from Bender can be used for ground fault monitoring. It gives alarm and trip contact according to the insulation values set by the user (insulation between ground and phase in kOhm or MOhm). These changeover contacts can be taken into CU as DI and then can be used as wished. Please refer to the attachment for the bender relay information. Regards Shahid AttachmentINSULATION MONITOR.PDF (182 Downloads) |
Follow us on