5/6/2021 7:30 AM | |
Posts: 24 Rating:
|
Same question. Any idea? Thanks, Laura |
5/6/2021 9:38 AM | |
Joined: 4/28/2015 Last visit: 9/27/2023 Posts: 3259 Rating:
|
Hi, sorry, I missed to answer this.. I think the only way is to enable this module in the kernel. So I'd try to add CONFIG_RTL8188EU=m to iot2050_defconfig_extra.cfg and start building the image. You can also open an issue on github, with the request to add this USB WiFi dongle to the supported ones. Best regards! |
Follow us on