4/7/2014 7:47 PM | |
Joined: 5/13/2012 Last visit: 1/17/2024 Posts: 179 Rating: (1) |
hii mike please help me , now i have got a new information which is this workstaion has a digsi software and the client would like to communcat with siprotic devices 7sj63,7sj64 using IEC 103 using a stare couple IEC 103 RER 125 fiber optics connection ST type . he would like to see disturbance record through iec iec 103 using digsi software so what setting should i use ?see attched pic,because i am doubt about systmport and service port, thanks and best regrads AttachmentFull page photo1.pdf (64 Downloads) |
Last edited by: fanana at: 4/7/2014 8:14 PMbest regards |
|
4/24/2014 11:53 AM | |
Joined: 5/13/2012 Last visit: 1/17/2024 Posts: 179 Rating: (1) |
dear mike thnak you very much for your answer 1- i would like to clarify something ,when you say digsi network you mean network using( mini star coupler siemens ) is it ok or not . 2-the customer give me a connection diagram to our siprotics devices ,connect all our devices by RER 125 ABB master 103 ?!!! connected to the ELICS station ,according to the attached pdf can i use the service port to open digsi ?!!! i am confused , i understand your answer before 3-you said that i can use SICAM PAS ,whcih version can i use i think it would be v 8.02 or not and what licensce should i select ,IEC 103 master ??or what Attachmentsupport.pdf (73 Downloads) |
best regards |
|
4/24/2014 12:09 PM | |
Joined: 5/13/2012 Last visit: 1/17/2024 Posts: 179 Rating: (1) |
see also my MLFB What about if i receive the fault record at working station which support IEC 103 ,what kind if program can i open this record??? Or should i install sigra on it?
Attachmentsupport2.pdf (62 Downloads) |
Last edited by: fanana at: 4/25/2014 12:59 PMbest regards |
|
Follow us on