6/16/2013 9:39 AM | |
Posts: 49 Rating: (0) |
hello everyone ! i am trying to send e-mail through wincc, i have some questions regarding my task : 1> smtp server is necessary for it, means can we send email direct through scripting ??? 2> if smtp is necessary for it so please share link where it can be download easily ... 3> i am trying this script :
is there any thing wrong in this script if yes make plz correct or point it |
6/16/2013 10:12 AM | |
Posts: 1064 Rating: (72) |
1) yes you can send mail through scripting 2) smtp server is neccasary or the infomation to connect to your company mail server , search the internet there a lot of simple smtp server available for free 3) the script does work as i had it on a wincc project sending emails at a set time and on demand |
6/16/2013 10:23 AM | |
Posts: 49 Rating: (0) |
in smtp server dns server is written, what does it mean ?? |
6/16/2013 10:41 AM | |
Posts: 1064 Rating: (72) |
Take a look at this it might help you understand more http://en.wikipedia.org/wiki/Simple_Mail_Transfer_Protocol |
6/16/2013 11:05 AM | |
Posts: 1064 Rating: (72) |
/tf/WW/en/Posts/2568 Take alook at this pay attention to the one from Nemo this script works well if you are using a corprate email server and have Office installed but it has to be 2003 or older for the script to work or you will run into problems with security for office |
6/11/2015 7:33 AM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
So it works now? does it really depends on http://schemas.microsoft.com/cdo/configuration/ (gives an error opening that link in a browser?) For your information, I used Blat (Open Source), a Windows Command Line SMTP Mailer. This can also be used from inside VBScripts. http://sourceforge.net/projects/blat/ |
B r g d s , |
|