1/20/2014 7:11 AM | |
Joined: 3/20/2013 Last visit: 3/21/2025 Posts: 676 Rating:
|
You are working with CP343-1 or with the advanced version? you are writing both names. If you have the CP343-1 advanced pls go with the following manuals: - chapter 5.6 - chapter 8 (Kommunikation über AG_SEND/AG_LSEND) There is also an helpful application for going with your CPU and sending mails: Sending of Emails to SMTP Server with a S7-CPU This is the part for the side of the PLC. You have, of course, to adjust your mail server and have the opening of the Mail Port, etc... in your IT infrastructure. |
Best Regards, |
|
Follow us on