Industry Online Support
Technical Forum
8/17/2017 5:02 PM | |
Posts: 1 Rating: (0) |
Hello, I am having trouble selecting a mapping file from the interface settings of a SIPROTEC 7SJ64 in DIGSI 4. I am using a "DNP IP / IEC 61850" and a "IEC 61850, Fibre EN100" communications modules. From what I have read in the DNP IP Communication Module PDF, I should be able to select a DNP mapping file. Is this possible using these modules? Can anyone please advise how I can map binary inputs/outputs to DNP points while using the DNP IP / IEC 61850 and IEC 61850, Fibre EN100 modules? I've attached screenshots for reference. Thank you AttachmentScreenshots.zip (90 Downloads) |
Follow us on