8/8/2018 7:25 AM | |
Joined: 10/11/2006 Last visit: 2/3/2023 Posts: 5412 Rating:
|
Hello, please refer to parameter p0491 "motor encoder fault response", where you can set "1" or "5" which means in case of encoder fault the drive switches to encoderless operation (in case of "5" with an additional alarm message). Please note, that the encoderless operation has to be setup correctly as shown in the function manual. |
With best regards, |
|
Follow us on