5/11/2006 3:29 PM | |
Posts: 36 Rating: (3) |
Is it possible to enable / disable keys in runtime (ex. Alt+Tab) in a WinCC cliente by Password check level permition? If so how can I do it? Thanks |
5/11/2006 4:57 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
lkkezelf's method will work or youcan use C scripts. See http://support.automation.siemens.com/WW/view/en/13406395for an example project. |
5/11/2006 5:14 PM | |
Posts: 36 Rating: (3) |
Thanks That's exactly what I wanted. |
1/10/2008 2:44 PM | |
Posts: 13 Rating: (0) |
The link: http://support.automation.siemens.com/WW/view/en/13406395 doesn't work. Can anyone put the script in the post? Thanks |
1/17/2008 9:49 AM | |
Joined: 9/1/2005 Last visit: 12/5/2024 Posts: 4114 Rating: (195) |
Hello fremen1430, contacting our "FAQ-Team" I got the information that the entry is replaced. The new one is for free and should be found here: How can you have event-triggered locking/releasing of Windows key combinations at Runtime? Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on