10/18/2011 7:57 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Take a look at http://support.automation.siemens.com/WW/view/en/45977588 concerning wiring and example project. Give us the type of encoder in order to see if it is match with reading module. Best regards, Hristo Mihalev |
10/18/2011 8:48 AM | |
Joined: 9/8/2010 Last visit: 8/7/2024 Posts: 30 Rating: (0) |
Dear Sir, i want to detect pulses of an encoder in my application. Right now i am working on the configuration of the project with CPU31 5 2PN/DP and 1SI 5v/500khz module for counting. now i dont have encoder. i am trying to see the count by giving 5V pulses externallyto terminal 1 0r 3 of TM E 30S-44-01.Is this correct procedure?is there any sample program for the reference.I have developed the attached prg with the help of manual ET 200S Technological Functions page no 121.please guide me.
Attachment5v_500khz.zip (409 Downloads) |
Last edited by: manko at: 10/18/2011 8:56 AM |
|
10/18/2011 9:32 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Try attached FC. I hope will works. Just connect your PIW number and... Best regards, Hristo Mihalev AttachmentSSI.zip (420 Downloads) |
Follow us on