7/26/2022 8:16 AM | |
Joined: 4/28/2009 Last visit: 8/12/2024 Posts: 347 Rating: (43) |
Hello, in technical data for CU250S-2 there are output voltages for encoder interfaces. Terminal 33 is 24V power source for HTL encoders with max.current 200mA, Sub-D connector has 24V power source on pins 4 and 5 with max. current 350mA. Try to check correct connection of your encoder to terminals/Sub-D connector. If you use also basic positioner, there are permissible encoder combinations, described in Basic positioner function manual in chapter 4. With regards Martin |
Follow us on