10/15/2017 9:54 PM | |
Joined: 9/27/2006 Last visit: 3/21/2025 Posts: 12344 Rating:
|
Hello Rakib; One very valuable suggestion we can make is for you to do a bit of research on the communication possibilities for each of these powermeter families. For example, rthe Sentron PAC3200 support Modbus TCP: --Deleted Link-- Both the PM1200 and the M2M support Modbus RTU (RS-485); I will let you look on the web for the appropriate documentation. The Converz 5240 powermeters, on the other hand, need an add-on modue for Modbus RTU: --Deleted Link-- If all is correct, then you would need 2 networks: one Ethernet (for Modbus TCP) switch every 100m, and a RS 485 serial bus for Modbus RTU. Since some of the power meters only go to 19,2 kB they can easily carry the signals over 300m on a shielded twisted-pair line. So then you have to think of the CPU you will use. A S7-1200 for example supports Modbus TCP on its integrated Ethernet portsd and has Modbus TCP functions available. You would need a serial communication module for RS 485 if you want to implement Modbus RTU. Search for this information on the foeum, using the seach box at the top right of this page. To help you further we would need a schematic of your plant, with the distances of each slave. Hope this helps, Daniel Chartier AttachmentPDF files.zip (198 Downloads) |
Last edited by: Jen_Moderator at: 10/19/2017 8:13:06 AMAdded PDF files as an attachment. |
|
10/17/2017 8:12 AM | |
Joined: 9/28/2017 Last visit: 11/4/2024 Posts: 64 Rating:
|
Thanks for the answer. Is there any way to connect all Modbus rtu devices through modbus tcp protoco? |
10/17/2017 3:18 PM | |
Joined: 8/3/2009 Last visit: 3/21/2025 Posts: 15056 Rating:
|
Hello RAKIB Do you also need help in Siemens communication to the PAC3200? Perhaps this could help: https://support.industry.siemens.com/cs/ww/en/view/40614428 Bye Muof |
If this Information really helps, you could use the Rate function |
|
10/31/2017 7:44 AM | |
Joined: 9/28/2017 Last visit: 11/4/2024 Posts: 64 Rating:
|
Dearola84, Thanks a lot for your answer. I would really like to be helped. It will be a great pleasure if you have time to help me. I am giving you the information of the devices that i have to integrate as well as the hardware & software list i have chosen for the project. if you provide your e-mail address / other contact info then i will be able to share more about the project. Hope to hear from you soon. Thanks a lot. best regards Rakib Attachmentenergy meter project info.zip (181 Downloads) |
10/31/2017 7:55 AM | |
Joined: 9/28/2017 Last visit: 11/4/2024 Posts: 64 Rating:
|
Dear ola84, Here is the plant 1 & 2 network arrangement i thought. Please find the attachment.These are two different project. I mean there is two office for plant 1 & 2. There is no connection between plant 1 & 2. first i have to complete plant 1 and then 2. Thanks. Regards rakib Attachmentnetwork arrangement plant 1 and 2.zip (195 Downloads) |
Follow us on