6/27/2013 9:47 AM | |
Posts: 72 Rating: (2) |
hi, can you give your model no.. if it is DP slave GSD file must. no need sfc
|
6/27/2013 10:08 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi jolter ggg, Give us the model of the energy meter, and explains to us what you want to use Profibus or Modbus? |
6/27/2013 10:22 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi jolter ggg, You need a GSD file of the energy meter and a Profibus module, you have this? |
6/27/2013 10:27 AM | |
Posts: 49 Rating: (0) |
no i dont have gsd file and can u tell me from where i can download it |
6/27/2013 10:57 AM | |
Posts: 262 Rating: (45) |
Hi, Why dont you ask your distributor to replace this unit with Advanced Siemens PAC 3200/ 4200 devices. These devices have inbuilt library in SIMATIC PLCs and import of GSD files becomes unnecessary. For more details about PAC, kindly refer... https://w3.usa.siemens.com/us/internet-dms/btlv/access/access/Docs/SENTRON_pac3200_manual_ul_PSC_en.pdf?HTTPS=REDIR and also please refer the an old fourm link which will help you:- /tf/WW/en/Posts/21539 |
6/27/2013 11:10 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi Valli, We are talking about an energy meter (Pilot PMAC 735) not energy meter SIEMENS SENTRON PAC 3200 or 4200. |
6/27/2013 11:16 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
The order number must/should be PMAC735-P-x-x in order to be sure profibus module is installed. |
6/27/2013 11:39 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi jolter ggg, No you can not, you need its GSD file. |
6/27/2013 11:41 AM | |
Posts: 49 Rating: (0) |
yes UMENCHO i have pilot pmac 735 p model , i am sured this is profibus supported. see in it ( http://en.pmac.com.cn/Products_show.asp?lan=zh-en&skin=2&newsid=125948036 ) |
Last edited by: jolter ggg at: 6/27/2013 11:42 AM |
|
6/27/2013 11:49 AM | |
Posts: 262 Rating: (45) |
Ya i know he is trying with Pilot meters but my suggestion was replacing it with PAC. Anyways... i went to their website and found a few contact information to get GSD for profibus:- http://en.pmac.com.cn/sort.asp?lan=zh-en&skin=6&enterid=6&searchsub=1&id=20 Kindly contact them to get the desired info... this is not a integration issue and hence helping to you would be limited. |
This contribution was helpful to1 thankful Users |
6/27/2013 11:54 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi jolter ggg, |
Follow us on