1/15/2013 1:11 PM | |
Posts: 15 Rating:
|
Hello boys, this solution is exactly what I need for measuring differences between two electricity phases: - P1 - First phase from solar power system - P2 - Second phase from consumption of house If P1 - P2 > 200W (exces of FVE), then switch on some equipment in house (heater, batery charging, etc.) (its the same as your heating system - T2-T1) I have two elektro meter with pulse outputs (2000 imp/kWh) and I have to comparate time between pulses and from this time then calculate actual consumption in kWh (for example 5 sec. betwen pulses = (2000imp/3600sec)×5sec=2,778kWh I guess i should use your program, or bigger part of it, but i have S7-1200 1214 DC/DC/RLY, is there any possibility to use your program with TIA V11 SP2? Thank you very much. |
Last edited by: O_Moderator at: 1/17/2013 11:16 AMnew subject after splitting from /tf/WW/en/Posts/25664#top |
|
Follow us on