6/30/2016 1:46 PM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (193) |
Hello N.V.Bala, this can help you with multiple line Input/output in HMI: https://support.industry.siemens.com/tf/ww/en/posts/151548/ I don't understand what you mean with multiple lines in the string from PLC. How are the lines seperated? Some special character? |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
6/30/2016 4:12 PM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (193) |
Hello N.V.Bala, I don't know if it works, but this might be a possibility:
The other way would be to slice the string up into smaller strings (using the PLC or an HMI VB-Script). You could use an arry of string, maybe? Then you write into more than one I/O-field (and don't show the borders, so it looks like one block). |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
Follow us on