2/9/2007 8:35 AM | |
Posts: 20 Rating:
|
Hello. I found some error entries in WinCC log files, but I don't know what they mean. Can anybody help me? System consists of redundant server pair and a client. Error entries are in the server log file. I'm far away from the system now, so it's difficult to check what actually happens there. I haven't received any complains from users, so I think that everything works fine there, but repeating error in log file is no good. The error is: ArchiveManager,Failed to switch archive(Type:1):(null) ! It is repeating every day at 23:55. I attached fragment of file. Thanks in advance. AttachmentWinCC_Sys_04_fragment.zip (94 Downloads) |
2/9/2007 9:31 AM | |
Posts: 3149 Rating:
|
Hi please attach all logfiles, is your WinCC redundancy working without problems? nemo |
2/9/2007 10:21 AM | |
Posts: 20 Rating:
|
Here are all the log-files. Unfortunately, I have logs from one server only. Log-files contain more other errors (there are some problems with OPC connectivity), but I think these errors are not related to archiving system. Thanks in advance. AttachmentDiagnose SIKN Server№1.zip (75 Downloads) |
2/9/2007 12:35 PM | |
Posts: 1275 Rating:
|
Hi! About the failed to switch archive, check this out. What is your WinCC version? There also this post. There are some errors in your log files which seem to show quite a lot, such as: 255,04.11.2006,13:52:09:096,1003082,4,Administrator,WCCSRV1,NRMS7PMC,MldReceiveMsg: RDFT_EVT_PMC_ALARM_S(Q) Connection 'ASU': Insufficient S7-memory - Message overflow from AS detected 255,31.01.2007,10:05:05:979,1007000,4,,WCCSRV1,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,12.11.2006,15:36:52:756,1003079,4,user,WCCSRV1,NRMS7PMC,Zusatzwerte: unbekannte Kombination Datenart und Lange from connection 'ASU' datatype = 4 and length = 96 ([:o]I don't know what this one means) 255,28.09.2006,22:32:51:291,1007001,4,,WCCSRV1,SCRIPT,ExecuteError in Action @98 255,29.09.2006,16:43:14:471,1000005,4,admin,WCCSRV1,DataManager Runtime,Format error of tag 'IVK/meanP1h.mean'. Format ID: 136314880 = 8200000(hex) gscrt.exe : 04.11.2006 12:44:35 : SIMATIC HMI WinCC (GlobalScript Runtime): Error :Error at GTI APEndAct Undefined error. 2006-11-10 08:35:00,600 ERROR ...herrors[425] CPPN/Sign_tr2_reset- ERROR c0040007 2006-11-10 08:35:00,600 ERROR - ChannelUnit::SysMessage("[OPC Groups (OPCHN Unit #1)]![ASUCPPN]: AddItem "CPPN/Sign_tr2_s" failed, error=c0040007 (The item is no longer available in the server address space)") 2006-11-11 14:48:36,066 ERROR ..FOPCData::InitOPC QueryInterface(IID_IOPCServer)- ERROR 80070005 2006-11-11 14:48:36,066 ERROR - ChannelUnit::SysMessage("[OPC Groups (OPCHN Unit #1)]![ASUCPPN]: QueryInterface IOPCServer for \\ASUCPPN\OPCServer.WinCC failed, Error=80070005 (HRESULT = 80070005 - E_ACCESSDENIED (Access is denied.))") You should clear those out as well... |
Last edited by: Danielle at: 2/9/2007 12:41 PMLast edited by: Danielle at: 2/9/2007 12:37 PM |
|
2/9/2007 12:40 PM | |
Posts: 3149 Rating:
|
Hi thanks Danielle, I am getting old....couldn´t remind that this question has already been asked [:D] nemo |
2/9/2007 1:34 PM | |
Posts: 3149 Rating:
|
Hi, perhaps this FAQ can answer your question? http://support.automation.siemens.com/WW/view/en/2357302 nemo |
2/9/2007 2:02 PM | |
Posts: 20 Rating:
|
No, unfortunately this FAQ doesn't give any explanation about whether Dynamic Displays are included in 5000 or not. |
Follow us on