Industry Online Support
Technical Forum
5/6/2014 2:54 AM | |
Joined: 7/15/2008 Last visit: 4/21/2023 Posts: 382 Rating:
|
Hello fmgl There are several reasons why the BSAP light is on. -- PLC Stop activated ( Program or Hardware Error ) -- Power Supply Monitor Input is connected or has no supply voltage -- .................... but without a Laptop and a look at theISTAK or BSATCK it is very hard to diagnose from here. Please see link below for the 928 Manual for some more info and on how to do a Overall Reset. http://support.automation.siemens.com/WW/view/en/1085837 Regards / m.f.g |
Follow us on