2/4/2020 10:03 AM | |
Joined: 4/22/2018 Last visit: 11/23/2024 Posts: 57 Rating:
|
Dear All, I am going to save some data in a text file on a SD card and use "With SIMATIC WinCC (TIA Portal) on a panel, how do you access process data in a file via a script?" Topic. I have downloaded the example and when I wanted to simulate it on PC, the following error occurred, "Error #429 ActiveX Component can't create object". I searched forum and understood the error is due to difference in operating system (Windows CE for the panel and Windows 7 for my PC). The File Control scripts are different in windows CE and windows 7 and the example used windows CE scripts. Am I right? I am going to download my project on a TP1500 but I want to check and debug it on the PC before download it on the panel. Is there any method for simulation on PC without any error? Bests |
Last edited by: Jen_Moderator at: 02/04/2020 13:12:56Optimized link. |
|
3/13/2021 12:37 PM | |
Joined: 2/12/2018 Last visit: 9/26/2023 Posts: 22 Rating:
|
Hello Ali
Differences between the VB script functions of Windows and WinCEhttps://support.industry.siemens.com/cs/cn/en/view/13408815 |
Last edited by: Jen_Moderator at: 03/15/2021 10:08:46Optimized link. |
|
Follow us on