5/12/2015 8:50 PM | |
Joined: 4/11/2014 Last visit: 5/30/2023 Posts: 2 Rating:
|
Good evening! I have some problems, Error: Application HMIRTM.EXE encountered a serious error and must shut down with TP900. The CPU is 315 PN/DP, the conecction network is a profinet. The compilation was ok, and also the transfer in HMI. Everything worked out, until the error ocurred and i was not able to do anything. I had to shut it down; when i started it again, it normally functioned, then after some time the error appeared. Has anybody found this problem and what has he done to solve this? If you can help me, i would be very glad. Thank you and i am waiting for your answer with a lot of interest. ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 5/13/2015 3:54:45 PMNew subject after splitting |
|
This contribution was helpful to
1 thankful Users |
11/30/2015 6:20 PM | |
Joined: 4/11/2014 Last visit: 5/30/2023 Posts: 2 Rating:
|
Good evening! I have solved the problem with the "'Error: Application HMIRTM.EXE encountered a serious error and must shut down with TP900''. It was caused by variable STRING from HMI, TP900; sometimes, when i wrote it in HMI, the variable was too long, because i used pieces of information from two STRINGs, together sent from PLC, CPU315-2PNDP. I hope this information will be usefull. |
This contribution was helpful to
2 thankful Users |
1/3/2020 8:56 AM | |
Joined: 4/28/2015 Last visit: 6/20/2023 Posts: 5 Rating:
|
Hi, have you solved your problem with Runtime crashing? |
8/12/2020 9:12 AM | |
Posts: 1 Rating:
|
I also encountered such a problem. How did you solve it in the end? Thank you very much.i am chinese,can"t speak englishi fluently |
9/4/2020 5:45 AM | |
Posts: 1 Rating:
|
Well, but I can see that you wrote in English. You don't have to speak it fluently. With a little bit of Baidu Translator, I guess it won't be too difficult to you. Hope you have figured it out anyway? |
11/27/2020 7:34 AM | |
Joined: 2/23/2017 Last visit: 4/12/2023 Posts: 1 Rating:
|
I have the same problem |
3/6/2021 1:31 PM | |
Joined: 2/21/2019 Last visit: 10/6/2022 Posts: 3 Rating:
|
não entendi , como você conseguiu resolver esse problema ? desde já grato ! |
Follow us on