Industry Online Support
Technical Forum
7/7/2014 5:12 PM | |
Posts: 311 Rating: (3) |
Hello, I got the following error, see below. What do I need to do ? Regards Per Olof |
7/8/2014 7:09 AM | |
Posts: 1299 Rating: (135)
|
Hello, click on the arrow in the column "go to". It will go to the tags which cause the problem. K!ke |
7/8/2014 8:56 AM | |
Posts: 311 Rating: (3) |
Thanks K!ke, but I could not solve the problem so I revert back to a saved version. The tags is not mine, it comes from TIA system!!! |
7/8/2014 12:58 PM | |
Posts: 1299 Rating: (135)
|
Hello, do you know which step caused the problem? K!ke |
7/8/2014 2:27 PM | |
Posts: 311 Rating: (3) |
Sorry I do not know. It was the HMI compile that got the errors. I have send the log to siemens. |
Follow us on