12/20/2022 7:19 PM | |
Joined: 5/6/2022 Last visit: 4/30/2025 Posts: 588 Rating:
|
Hi goudarzi91, First of all I think it would be interesting if you could please attach a screenshot of the error you are encountering. On the other hand, to be able to see if the error is from the project or from the software you have installed, you can do some small tests: - Delete the IM mask from the project and re-compile and test the simulation. Here is the link on how to do it. -> "How do you delete the IM folder of your TIA project - Create a new very simple project and try to simulate it to see if it also closes and gives you a failure in the simulation. I look forward to hearing from you to see how we can solve your problem. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
12/21/2022 6:10 AM | |
Joined: 5/11/2022 Last visit: 4/30/2025 Posts: 73 Rating:
|
hello sir, I have done it before, but when I active ( runtime setting >> service >> alarm logging in runtime or date logging in runtime ) running wincc was interrupted and Deactived after 1 second since active simulation. |
Last edited by: goudarzi91 at: 12/21/2022 09:18:48 |
|
12/21/2022 1:19 PM | |
Joined: 5/11/2022 Last visit: 4/30/2025 Posts: 73 Rating:
|
thanks alot sir I deleted IM folder from the project after that I recompiled from my project but the problem didn't solve. I created a new simple project and I run the simulation again but it failed. I don't know really what should I do? |
Last edited by: goudarzi91 at: 12/21/2022 13:20:17 |
|
12/21/2022 7:10 PM | |
Joined: 5/6/2022 Last visit: 4/30/2025 Posts: 588 Rating:
|
Hi goudarzi91, Having checked these points and if the same thing continues to happen, the following points come to mind: 1. As it happens when you select the Alarm Logging service, I would comment that you should check the AlarmLogging configuration to see if you are exceeding the established limits. At the configuration of the AlarmLogging you must check that you meet the following conditions: - Total size of the segments, maximum 6 months. - Total sum of segments in ArchiveManager (Alarm Logging + Tag Logging (Fast + Slow)) not exceeding 200 segments. - Each segment no more than 2GB. 2. Maybe it could be related to some compatibility issue. You could share the following with us?: - Screenshot of the exact operating system version. To do this, you can type "winver" (without the inverted commas) in the Windows search engine and send us a screenshot showing which version and build you get. - Screenshot of the Siemens software installed on the PC. To do this, take a screenshot from TIA Portal -> Help -> Installed Software. Which version are you using? You can also check it yourself from the free siemens 'Compatibility Tool'. 3. Finally, you can also try performing a repair of the installation. This may fix problem with the installation. Best regards! |
Last edited by: ElonksuM_SN_BN at: 12/21/2022 19:15:03If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
12/22/2022 5:11 AM | |
Joined: 5/11/2022 Last visit: 4/30/2025 Posts: 73 Rating:
|
hello sir I was so pleased to hear from you. there is a picture that show version of software program installed on my pc and operation system version and the configuration of alarm logging in my project. |
Follow us on