Industry Online Support
Technical Forum
2/5/2010 6:58 AM | |
Posts: 88 Rating:
|
Hi daga, Thank you! Here is the right OS log. T41 |
2/5/2010 7:30 AM | |
Posts: 88 Rating:
|
Hi, 1. I'm not sure why it mentioned the language. This is a test project. I just want to use "English". 2. My intention is a entire compile. Here is the OS compile log file. Thanks! T41 The log is a txt file. But I can't upload this kind of file. So use zip file. AttachmentTRANSFER_compile_OS.zip (44 Downloads) |
2/5/2010 9:06 AM | |
Joined: 4/5/2006 Last visit: 6/25/2024 Posts: 917 Rating:
|
Hi T41 , seems you did a very simple project, this error happens with this project ONLY ? did you tryied to create a new one (empty maybe) with wizard, compile AS then compile OS and see what happenes? it's work fine or same trouble? if you got trouble again, try to post what installed on you PC (application from windows control panel and SW installed from Siemens utiliy regards |
Follow us on