8/26/2014 6:20 AM | |
Posts: 3 Rating:
|
Dear all, I have an error on FB80 (as attachment PLCB is ok, but PLC A have a fault). Event code on CP341 is 0E56 that means FB can't initial. Can you help me to solve this problem. More detail: protocol modbus is slave AttachmentError FB.pdf (267 Downloads) |
8/26/2014 12:07 PM | |
Posts: 1368 Rating:
|
Hello, your FB80 returns also an error code: ERROR_NR = 2 ERROR_INDEX:301 (status of P_SND_RK) Status of P_SND_RK: Invalid source/destination data type or area does not exist (start address, length) Invalid or no DB (e.g. DB 0) or Other data type invalid or missing Interprocessor communication byte number invalid or Invalid interprocessor communication flag bit number or 'S' or 'F' was not selected |
2/25/2016 2:12 AM | |
Joined: 4/22/2009 Last visit: 11/28/2022 Posts: 19 Rating:
|
The link is yours I can't access. Can you advise any solution for this case? |
2/25/2016 12:54 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by duongvuquy is split to a separate thread with the subject Honeywell master can't write single coil. Best regards |
Follow us on