6/27/2011 12:09 PM | |
Posts: 13 Rating: (0) |
Hi Guys I'm getting a similar message trying to import a block from one progranm to another with SFB1 used as the up/Down counter. I'm getting the Error Message "E:The multiple instance block FB504 cannot be imported because the corresponding block SFB1 was modified.". I've checked the time stamps and edited FB504 to remove references to SFB1 and Still I'm getting the same issue. I've tried updating interfaces etc. but some of the menu options shown here and on other posts do not seem to be available to me. (I.E in the Options --> Charts menu in component view, the only option available for me is "Settings for Copying/Moving") I'm unfortunately being forced to use PCS7 V5.1 on S7 Version 5.1 on this project so upgrading (Or even Getting rid of PCS7 completely) is not an option. Any Help or Suggestions would be greatly appreciated. Thanks in advance Alan Splitted from The multiple instance block FB1044 cannot be imported because the corresponding block FB1046 was modified.. |
Last edited by: O_Moderator at: 6/27/2011 2:08 PMLast edited by: O_Moderator at: 6/27/2011 2:07 PMquotation added Last edited by: O_Moderator at: 6/27/2011 2:06 PMnew subject after splitting |
|