Industry Online Support
Technical Forum
10/15/2009 2:30 PM | |||
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi bronzon , are you migrating from v5.x to v7.x directly?..or from v5.x yto v6.x, then from v6.x to v7.x? here a previuso link about related forum question
Are you using PCS7 standard library? any prpofibus PA or something else? (in past time i had trouble because older PA block library sometimes doesn't support "Profile 3", maybe not for PA but you could have something like that) If everything alright can you try to perfom a "Save AS" in original project to be sure is error free? If need more help, try to explain about your HW congihuration, custom ot thirdy part library and so on. More ppl could help Regards |
||