11/26/2007 4:25 PM | |
Posts: 124 Rating: (17)
|
Please verify these two links. I guess they'll help. |
12/3/2007 8:49 AM | |
Posts: 124 Rating: (17)
|
Hello Enigma/Anirban Enigma is right. Thank you for your answer, Enigma. Last week I have exactly the same problem and to fix it I had to create several groups in OB100. In fact this response is in one of the links I tried to send (in the link below, but it didn't work the first time) Too many block instances in a runtime group In either case the error messages occur because there are too many block instances integrated directly in a task. As a result, the FC to be generated by the SCL compiler may exceed the maximum permitted size of 64 KB. Remedy: Here is the link again (I hope it works now). It's FAQ 771569 Why does the error message "Maximum length of code area reached (max. 64 KB)" or "Insufficient main memory" appear when the CFC charts are compiled? https://support.automation.siemens.com/WW/skm/frameset.asp?url=%2FWW%2Fllisapi%2Edll%2F771569%3Ffunc%3Dll%26objId%3D771569%26objaction%3Dcsopen%26siteid%3Dcseus%26skm%3D1%26lang%3Den&Query=Maximum+length+of+code+area+reached+%28max%2E+64+KB&SearchArea=alle&id=771569&F11Marker=true&siteid=csius&query2=&modelled=&lang=en |
Last edited by: Mario Bragança at: 03.12.2007 08:54 |
|
2/28/2012 4:23 PM | |
Posts: 133 Rating: (9) |
Thanks for your experience . It helped me to resolve this issue as well. |