9/30/2021 5:00 PM | |
Joined: 2/6/2015 Last visit: 3/21/2025 Posts: 132 Rating:
|
Hi Abdallah I have the same problem, but the settings on the RT server are the same. The problem has began after i have installed on the RT server the TIA_UMC_V2 from the TIA Portal V17 DVD-2 My Runtime is V16Upd4. I don't know if that is the reason, but the error came definitly just after the installation. Do you have an idea? I have contacted Siemens but got not any answer yet. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/01/2021 08:09:40New subject after splitting Last edited by: Jen_Moderator at: 10/01/2021 08:12:31Removed embedded image because it is crossed out in the open topic. |
|
10/1/2021 8:10 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
Closed cause question posted twice. The second thread with the subject SWAC Login Error after installation of TIA_UMC_V2 on RT server is published within the conference WinCC Unified Systems. Jen_Moderator |
Follow us on