6/29/2016 4:46 PM | |
Posts: 171 Rating:
|
I am using 6ES7972-0EA00-0XA0 to connect with S7 1200 thru TIA v13. I have configured these parameters: TS Adapter WAN IP (Available IP in the industry) IP 192.168.2.228 SUbnet 255.255.255.0 gateway 192.168.2.11 DNS 8.8.8.8 TS Adapter LAN IP 192.168.1.20 Subnet 255.255.255.0 (no gateway) Service PC IP 192.168.1.30 PLC IP 192.168.1.(1to9) subnet 255.255.255.0 no gateway Still am getting error that TS adapter not available. Also attached the configuration. Help me!!! ------------------------------------------------------------------------------------------ AttachmentTS Adapter.docx (272 Downloads) |
Last edited by: santhosh sundaram at: 6/29/2016 4:48:56 PMLast edited by: Min_Moderator at: 6/30/2016 11:44:49 AMNew subject after splitting Last edited by: santhosh sundaram at: 7/2/2016 6:12:50 AM |
|
7/3/2016 9:21 AM | |
Posts: 171 Rating:
|
Anyway thankyou people. I got the reason and now am connected. |
1/25/2018 9:01 PM | |
Joined: 10/4/2017 Last visit: 5/1/2024 Posts: 2 Rating:
|
What you did my friend in order to solve the problem? |
Follow us on