3/5/2013 8:36 AM | |
Joined: 6/23/2008 Last visit: 1/23/2025 Posts: 1168 Rating: (283) |
Hello, is the time you want to transfer of type "TOD","TIMER"or "DT" ? Or ist just aREAL or INTEGERvalue which contains a count of seconds? If my first question is true, I think it is not possible to transfer the types TOD and DT directly to WinCC. Here is a way how to do that: Link In PCS7 you are usally not using timers. You create a time in your source codeusually by counting the calls with considering 'sample time' |
Last edited by: mark1507 at: 3/5/2013 8:38 AM"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
3/5/2013 8:43 AM | |
Posts: 5 Rating: (0) |
It looks like: time_variable {S7_m_c:='true'} : TIME := T#5s;
|
Follow us on