Industry Online Support
Technical Forum
6/28/2009 10:51 PM | |
Joined: 9/28/2005 Last visit: 12/27/2022 Posts: 2957 Rating:
|
Hello, You should open SQL server configuration manager from Start menu and be sure that SQL server is running. If not, please start it. Normaly it should run automatically, so it might be a problem with SQL installation. I have had the same problem as you and finding the solution for me took too long, so I uninstalled WinCC Flexible AND SQL server from machine. Then reinstalled WinCC Flexible and everything was ok. As I know from my experience, restoring broken SQL installations might be very painful, so best way is to do repair install (uninstall and then install again). You can also look at this FAQ http://support.automation.siemens.com/WW/view/en/29420407 It might be helpful |
Last edited by: Darius at: 6/28/2009 10:53 PMBest regards, |
|
6/30/2009 3:57 AM | |
Posts: 90 Rating:
|
Hello Darius ! Well the SQL servers config managerwas running, but the error remained. I uninstalledthe WinCC Flexible and SQL server from my laptop and installed them again butthe errorremained either. So, I reinstalled the STEP7Software and now all is ok !! Thanks for the help ! regards |
Last edited by: Denker at: 6/30/2009 7:30 AM |
|
Follow us on