8/16/2006 10:09 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
What version of WinCC do you have ? What happens if you print from the server ? |
8/16/2006 10:27 AM | |
Posts: 7 Rating: (0) |
I have WinCC V6.0 Incl. SP1. I didn't try to print from server |
8/16/2006 10:30 AM | |
Posts: 7 Rating: (0) |
In my PC a have 512 MB of RAM and when starting printing processor load is about 50 % (I have P4 processor with HT) |
8/16/2006 10:51 AM | |
Posts: 3149 Rating: (171)
|
Hi, well, you should anyway install an actual WinCC SP and some more RAM is never a mistake: http://support.automation.siemens.com/WW/view/en/22303359 Hyperthreading should be OK for WinXP but not for Windows2000 Just check your WinCC release note for more info.. nemo[:D] |
Last edited by: Nemo at: 8/16/2006 10:55 AMLast edited by: Nemo at: 8/16/2006 10:54 AM |
|
8/16/2006 12:50 PM | |
Posts: 7 Rating: (0) |
Post from Winncc_sys.log: 255,26.07.2006,08:23:57:217,1000203,4,technolog,KLIENT-2,DataManager Runtime,KLIENT-2Runtime deactivated on machine 'KLIENT-2' 255,26.07.2006,08:23:58:030,1007001,4,,KLIENT-2,SCRIPT,UnLoadFctAll nCount 358 255,27.07.2006,17:07:36:841,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,07.08.2006,14:56:14:193,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,08.08.2006,11:52:00:171,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,08.08.2006,13:29:00:252,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,09.08.2006,07:28:56:091,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,09.08.2006,08:09:46:123,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,09.08.2006,12:19:51:315,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,09.08.2006,13:35:31:373,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,10.08.2006,13:52:22:533,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,11.08.2006,08:21:33:056,1000203,4,MISTRZ,KLIENT-2,DataManager Runtime,KLIENT-2Runtime deactivated on machine 'KLIENT-2' 255,11.08.2006,08:21:33:791,1007001,4,,KLIENT-2,SCRIPT,UnLoadFctAll nCount 358 255,11.08.2006,13:46:41:669,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,14.08.2006,03:08:09:525,1007000,4,,KLIENT-2,SCRIPT,ActionOverflow:more than 5000 Actions to work Post from Winn_sstart.log: 255,26.07.2006,08:26:19:358,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project - pdlrt.exe - Status = LOAD DATA 255,11.08.2006,08:22:29:806,1007007,1,,KLIENT-2,SCRIPT,ProjectType 3 255,11.08.2006,08:22:31:759,1007007,1,,KLIENT-2,SCRIPT,DM_NOTIFY_PROJECT_OPENED 255,11.08.2006,08:22:45:697,1007007,1,,KLIENT-2,SCRIPT,new Runtime-Project 255,11.08.2006,08:22:45:869,1007007,4,,KLIENT-2,SCRIPT,before Read Standardfunction 255,11.08.2006,08:22:45:869,1007007,1,,KLIENT-2,SCRIPT,runtimeproject \\KLIENT-2\WinCC60_Project_Olsztyn\Olsztyn.mcp ok(getprojectdir) 1 255,11.08.2006,08:22:45:869,1007007,1,,KLIENT-2,SCRIPT,global c:\SIEMENS\WINCC\APLIB szProjectLibDir \\KLIENT-2\WinCC60_Project_Olsztyn\library\ 255,11.08.2006,08:22:46:119,1007007,1,,KLIENT-2,SCRIPT,count StandardFunctions: 339 255,11.08.2006,08:22:46:134,1007007,1,,KLIENT-2,SCRIPT,count StandardFunctions+ProjectFunctions: 358 255,11.08.2006,08:22:48:009,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project -- Text Library RunTime -- Status = START 255,11.08.2006,08:22:48:447,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project -- Text Library RunTime -- Status = SUCCESS 255,11.08.2006,08:22:48:447,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project -- Data Manager RunTime -- Status = START 255,11.08.2006,08:22:49:275,1000202,4,,KLIENT-2,DataManager Runtime,KLIENT-2Runtime activated on machine 'KLIENT-2' 255,11.08.2006,08:22:49:275,1000000,4,,KLIENT-2,DataManager Runtime,Runtime activated!!! 255,11.08.2006,08:22:49:291,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project -- Data Manager RunTime -- Status = SUCCESS 255,11.08.2006,08:22:49:306,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project - gscrt.exe - Status = START 255,11.08.2006,08:22:49:931,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project - gscrt.exe - Status = SUCCESS 255,11.08.2006,08:22:49:931,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project - pdlrt.exe - Status = START 255,11.08.2006,08:22:50:134,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project - pdlrt.exe - Status = LOAD DATA 255,11.08.2006,08:22:50:447,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project - pdlrt.exe - Status = LOAD DATA 255,11.08.2006,08:22:50:837,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project - pdlrt.exe - Status = LOAD DATA 255,11.08.2006,08:22:51:337,0,1,STOMIL,KLIENT-2,CCActivateDeactivate,WinCC Project Manager : Activate Project - pdlrt.exe - Status = SUCCESS |
8/16/2006 1:09 PM | |
Posts: 3149 Rating: (171)
|
Hi please solve your scripting problems with this FAQ http://support.automation.siemens.com/WW/view/en/2357302 nemo |
8/16/2006 2:10 PM | |
Posts: 7 Rating: (0) |
But is this scripting problem connected with my printing problem?? |
8/16/2006 2:38 PM | |
Posts: 3149 Rating: (171)
|
I´ve seen many strange effects with unsolved scripting errors |
Follow us on